AXIS#.HOME.SWITCHSOURCE

Description

AXIS#.HOME.SWITCHSOURCE selects which digital input will be used as the home switch. A value of 0 indicates no input is selected. If homing is started with a mode that requires a home switch, and AXISx.HOME.SWITCHSOURCE is 0, a fault is generated. Homing assumes the home switch input is normally 0 and will go to 1 while within a small window. You can use DIN#.INV to invert the signal.

Value Input Selected
0 No input selected
1-12 DIN1-DIN12
101-106 DIO1-106

  • When using DIO inputs the associated connector mode, X22.MODE or X23.MODE, must be set to GPIO mode and the DIO#.DIR must be set to input.

Versions

Action Version Notes
Implemented 02-00-00-000
Added DIO selections 02-09-00-000 R#43096 – Added DIO as additional sources to permit TTL input voltages for switch sources

General Information

This content is not applicable to KAS.

Type

Read/Write

Units

N/A

Range

0 (None), 1-12 (DIN1-DIN12), 101-106 (DIO1-DIO6)

Default Value

0 (None)
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
AXIS1.HOME.SWITCHSOURCE

5008h

0ah

Unsigned8

-

-

Read/Write

No

AXIS2.HOME.SWITCHSOURCE

5108h

0ah

Unsigned8

-

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.HOME.SWITCHSOURCE

6118

17E6

Unsigned8

Read/Write

-

AXIS2.HOME.SWITCHSOURCE

71654

117E

Unsigned8

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HOME.SWITCHSOURCE

6118

Unsigned8

Read/Write

-

Related Topics

Homing